2023-02-16 12:36 AM
in main call
platform_init_h12();
while(1)
{
lis2dh12_read_data_polling();
HAL_Delay(1000);
}
The read_data_polling.c code is as follows:
/* Includes ------------------------------------------------------------------*/
#include <string.h>
#include <stdio.h>
#include "lis2dh12_reg.h"
#include "stm32G0xx_hal.h"
#include "usart.h"
#include "gpio.h"
#include "spi.h"
#include "tim.h"
#include "IMU.h"
/* Private macro -------------------------------------------------------------*/
#define BOOT_TIME 300 //ms 5
#define CS_up_GPIO_Port GPIOB
#define CS_up_Pin GPIO_PIN_12
//#define SENSOR_BUS hspi1
#define SENSOR_BUS hspi2
stmdev_ctx_t dev_ctx;
lis2dh12_reg_t reg;
/* Private variables ---------------------------------------------------------*/
static int16_t data_raw_acceleration[3];
static int16_t data_raw_temperature;
static float acceleration_mg[3];
static float temperature_degC;
static uint8_t whoamI;
static uint8_t tx_buffer[200];
/* Extern variables ----------------------------------------------------------*/
/* Private functions ---------------------------------------------------------*/
/*
* WARNING:
* Functions declare in this section are defined at the end of this file
* and are strictly related to the hardware platform used.
*
*/
static int32_t platform_write(void *handle, uint8_t reg, const uint8_t *bufp,
uint16_t len);
static int32_t platform_read(void *handle, uint8_t reg, uint8_t *bufp,
uint16_t len);
static void tx_com(uint8_t *tx_buffer, uint16_t len);
static void platform_delay(uint32_t ms);
//static void platform_init(void);
/* Main Example --------------------------------------------------------------*/
void lis2dh12_read_data_polling(void)
{
/* Read samples in polling mode (no int) */
// while (1)
{
// lis2dh12_reg_t reg;
/* Read output only if new value available */
lis2dh12_xl_data_ready_get(&dev_ctx, ®.byte);
if (reg.byte)
{
/* Read accelerometer data */
memset(data_raw_acceleration, 0x00, 3 * sizeof(int16_t));
lis2dh12_acceleration_raw_get(&dev_ctx, data_raw_acceleration);
acceleration_mg[0] =
lis2dh12_from_fs2_hr_to_mg(data_raw_acceleration[0]);
acceleration_mg[1] =
lis2dh12_from_fs2_hr_to_mg(data_raw_acceleration[1]);
acceleration_mg[2] =
lis2dh12_from_fs2_hr_to_mg(data_raw_acceleration[2]);
sprintf((char *)tx_buffer,
"Acceleration [mg]:%4.2f\t%4.2f\t%4.2f\r\n",
acceleration_mg[0], acceleration_mg[1], acceleration_mg[2]);
tx_com(tx_buffer, strlen((char const *)tx_buffer));
}
lis2dh12_temp_data_ready_get(&dev_ctx, ®.byte);
if (reg.byte)
{
/* Read temperature data */
memset(&data_raw_temperature, 0x00, sizeof(int16_t));
lis2dh12_temperature_raw_get(&dev_ctx, &data_raw_temperature);
temperature_degC =
lis2dh12_from_lsb_hr_to_celsius(data_raw_temperature);
sprintf((char *)tx_buffer,
"Temperature [degC]:%6.2f\r\n",
temperature_degC);
tx_com(tx_buffer, strlen((char const *)tx_buffer));
}
}
}
/*
* @brief Write generic device register (platform dependent)
*
* @param handle customizable argument. In this examples is used in
* order to select the correct sensor bus handler.
* @param reg register to write
* @param bufp pointer to data to write in register reg
* @param len number of consecutive register to write
*
*/
static int32_t platform_write(void *handle, uint8_t reg, const uint8_t *bufp,
uint16_t len)
{
/* Write multiple command */
reg |= 0x40;
HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_RESET);
// HAL_Delay(1);
HAL_SPI_Transmit(handle, ®, 1, 1000);
HAL_SPI_Transmit(handle, (uint8_t*) bufp, len, 1000);
// HAL_Delay(1);
HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_SET);
return 0;
}
/*
* @brief Read generic device register (platform dependent)
*
* @param handle customizable argument. In this examples is used in
* order to select the correct sensor bus handler.
* @param reg register to read
* @param bufp pointer to buffer that store the data read
* @param len number of consecutive register to read
*
*/
static int32_t platform_read(void *handle, uint8_t reg, uint8_t *bufp,
uint16_t len)
{
/* Read multiple command */
reg |= 0x80;
HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_RESET);
// HAL_Delay(1);
HAL_SPI_Transmit(handle, ®, 1, 1000);
// HAL_Delay(1);
HAL_SPI_Receive(handle, bufp, len, 1000);
// HAL_Delay(1);
HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_SET);
return 0;
}
/*
* @brief Send buffer to console (platform dependent)
*
* @param tx_buffer buffer to transmit
* @param len number of byte to send
*
*/
static void tx_com(uint8_t *tx_buffer, uint16_t len)
{
HAL_UART_Transmit(&huart1, tx_buffer, len, 1000);
}
/*
* @brief platform specific delay (platform dependent)
*
* @param ms delay in ms
*
*/
static void platform_delay(uint32_t ms)
{
HAL_Delay(ms);
// osalThreadDelayMilliseconds(ms);
}
/*
* @brief platform specific initialization (platform dependent)
*/
void platform_init_h12(void)
{
/* Initialize mems driver interface */
// stmdev_ctx_t dev_ctx;
dev_ctx.write_reg = platform_write;
dev_ctx.read_reg = platform_read;
dev_ctx.handle = &SENSOR_BUS;
/* Wait boot time and initialize platform specific hardware */
// platform_init();
/* Wait sensor boot time */
platform_delay(BOOT_TIME);
/* Check device ID */
whoamI = 0;
lis2dh12_device_id_get(&dev_ctx, &whoamI);
if (whoamI != LIS2DH12_ID)
{
while (1)
{
/* manage here device not found */
lis2dh12_device_id_get(&dev_ctx, &whoamI);
if (whoamI != LIS2DH12_ID)
{
printf("LIS2DH12_ID = 0x%X\r\n",whoamI);
HAL_Delay(300);
}
else
{
printf("LIS2DH12_ID = 0x%X\r\n",whoamI);
break;
}
}
}
else //0x33
{
printf("LIS2DH12_ID = 0x%X\r\n",whoamI);
}
/* Enable Block Data Update. */
lis2dh12_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
/* Set Output Data Rate to 1Hz. */
// lis2dh12_data_rate_set(&dev_ctx, LIS2DH12_ODR_1Hz);
lis2dh12_data_rate_set(&dev_ctx, LIS2DH12_ODR_25Hz);
/* Set full scale to 2g. */
lis2dh12_full_scale_set(&dev_ctx, LIS2DH12_2g);
/* Enable temperature sensor. */
lis2dh12_temperature_meas_set(&dev_ctx, LIS2DH12_TEMP_ENABLE);
/* Set device in continuous mode with 12 bit resol. */
lis2dh12_operating_mode_set(&dev_ctx, LIS2DH12_HR_12bit);
}
2023-02-16 12:41 AM
Why hasn't the acceleration_mg changed?
2023-08-10 5:16 PM
I tried to debug this problem and found a simple solution, which is to manually increment the address by myself, as shown in the picture. Or use a driver that automatically increments the address.
2023-09-16 11:57 AM
Another solution is to enable register address auto-incrementation. It is enabled by adding value 0x80 to the register address. For example: i2cread(DEVICE_ADDRESS, OUT_X_L | 0x80, buffer, 6); to read 6 register bytes in one go, starting at address 0x28 (which is OUT_X_L).