2020-08-12 1:26 AM
Hi, my name is Vincenzo.
I am working with the ToF VL53L3CX. Lately I wrote some applications to make 6 sensors work. At first I thought that the applications were working well, but now I realized that if I set too high timing budgets I had a performance problem. Since when I work with only one sensor everything works correctly, I thought the problem was in the way I manage the 6 ToF.
For this reason, I was wondering if there was a project made by you where multiple sensors are managed.
Thank you in advance for your support.
Vincenzo
2020-10-13 12:12 PM
Hi Vincenzo,
Thank you for sharing your experiences with the community. Actually if there is no specific reason I would recommend to use the standard 100 Khz I2C instead of the fast mode (400 Khz).
Julien