cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to use new inclinometers for Earthquake monitoring?

Pasi MYLLYMAKI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Carlo LARGHI
Associate III

yes, it is. In the webinar an example has been provided: the recording of a moderate earthquake (ML 3.9) which happened in Milan while the IIS2ICLX was under long term testing. In general, IIS2ICLX has a noise density extremely low (so a very high resolution) and the capability of recording acceleration up to 260Hz with great resolution

View solution in original post

1 REPLY 1
Carlo LARGHI
Associate III

yes, it is. In the webinar an example has been provided: the recording of a moderate earthquake (ML 3.9) which happened in Milan while the IIS2ICLX was under long term testing. In general, IIS2ICLX has a noise density extremely low (so a very high resolution) and the capability of recording acceleration up to 260Hz with great resolution