2013-10-09 01:07 AM
Hi guys,
I just received a couple of iNemo M1 boards (http://www.st.com/web/en/catalog/sense_power/FM89/SC1448/PF253162). It's a nice little gem, and I look forward to design great stuff with it. However I have not managed to talk to it yet. So far I managed to upload iNEMOV2_Firmware_PackageV2.2.0_AHRS through USART, but I got no data when listening, and it was not recognized by the demo application.Looks like there are: iNEMOEngine_PW8, iNEMOEngine_Ll3, iNEMOEngine_PAAP and iNEMOEngine_Pl3P, but I could not find the files� Moreover my goal is to change the firmware, so I believe I need the Light version provided with sources.So in brief, is there a working firmware and demos somewhere? Is there firmware example sources somewhere? Should I use a different communication port?Thank you very much #inemo-m1-firmware-demos-source2015-01-08 08:36 AM