2022-07-16 09:34 PM
Hello ,
We are trying to interface the IIS328DQTR with STM32F4 MCU. Our code configuration steps are as below.
6.Wait for 500 ms.
Interrupt is not generated on INT1 line. When we read X,Y,Z axis register at 1 second, we are getting the constant value 0xE0E0.
Is there any issue in the configuration sequence? Are we missing any steps?
What should be the VDDIO pin configuration? Can we connect it to VDD directly?
Thank you.
2022-07-18 09:30 PM
I am facing this problem too.
No X,Y,Z data from the IC. SPI communication is working because I am able to read Who Am I register.
I am using STEVAL-MK1170V1 for IIS328DQTR
It would be really helpful if you can point out something.
Thanks