The forum board you are trying to access is permanently deleted.
2020-10-09 10:56 PM
2020-10-12 6:32 AM
Hi @Pzhen.1 ,
Used Google Translate, is the translation below correct?
I use 3.3V for the IIS2MDC device, both VCC and VDD_IO are 3.3V, and then use FPGA to read and write it, and I find that the SDIO output is 1.8V. Is this normal?
If so, I can say you that no, it is not normal. The SDIO high voltage has to be near Vdd_IO, so near 3.3V. I believe you should check if you are maybe measuring the average voltage on the output (3.3V/2 = 1.65V), or your application processor / master I2C / SPI (the FPGA) is powered at 1.8V.
-Eleon
2020-10-28 7:20 AM
Hi @Pzhen.1 ,
any update about this topic, from your side?
-Eleon