2018-03-09 12:37 PM
Hello,
I am trying to get both Interrupts 1 and 2 to trigger for two different movements and at different intervals of the time . But somehow only interrupt 2 is getting generated. Interrupt 1 is not getting called at all.
So, I wanted to check if interrupt 1 is getting generated from the IIS2DH in the first place. So, I removed the Interrupt 2 connection and had only interrupt 1. I used the same configuration that I used for Interrupt 2 generation for Interrupt 1 generation. Surprisingly, interrupt 1 was still not getting generated.
Below is my accelerometer configuration with Interrupt 2 only:
CTRL_REG1: 0x3F;
CTRL_REG4: 0x20;
INT2_CFG: 0x04;
INT2_THS: 0x05;
INT2_DUR: 0x01;
The above configuration worked perfectly with interrupt 2. When I used Interrupt 1 with the same configuration, it did not work. The configuration is as follows:
CTRL_REG1: 0x3F;
CTRL_REG4: 0x20;
INT1_CFG: 0x04;
INT1_THS: 0x05;
INT1_DUR: 0x01;
I don't understand why interrupt 1 doesn't generate for the same configuration for which interrupt 2 can work. Please help me.
Thanks
2018-03-12 2:35 AM
What do you mean by '
interrupt 1 doesn't generate'? Does it mean the signal on pin INT1 doesn't change, or do you only checks INT1_SRC and INT2_SRC registers.
To see signals on INT1 pin you have to enable it in CTRL_REG3 = 0x40 and similarly for INT2 pin CTRL_REG6 = 0x20.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.