cancel
Showing results for 
Search instead for 
Did you mean: 

If temperature drift needs to be calibrated after soldering externally, then together with the internal calibration we have a double drift calibration, which can easily work against each other.

Pasi MYLLYMAKI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Carlo LARGHI
Associate III

it is not recommended to apply an external temperature compensation, being the device already internally compensated over temperature. What it is suggested, in case of requirement of high accuracy, is to perform external calibration post-solder but at room temperature only (so not compensation at different temperatures)

View solution in original post

1 REPLY 1
Carlo LARGHI
Associate III

it is not recommended to apply an external temperature compensation, being the device already internally compensated over temperature. What it is suggested, in case of requirement of high accuracy, is to perform external calibration post-solder but at room temperature only (so not compensation at different temperatures)