I2C TXDR doesnt send the data on SDA. STM32F3 Discovery.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-07-03 5:04 AM
Posted on July 03, 2016 at 14:04
Sample program to get accelerometer data.
#include ''stm32f3xx.h'' // Device header
void
initSystem()
{
// LSM303DLHC wiring: SCL to PB6, SDA to PB7.
// Enable port B timing and set pins to alternate function mode. No pull-up/pull-down.
RCC->AHBENR |= RCC_AHBENR_GPIOBEN;
GPIOB->MODER |= GPIO_MODER_MODER6_1|GPIO_MODER_MODER7_1;
GPIOB->OTYPER |= GPIO_OTYPER_OT_6|GPIO_OTYPER_OT_7;
GPIOB->PUPDR &= ~(GPIO_PUPDR_PUPDR6 | GPIO_PUPDR_PUPDR7 );
GPIOB->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR6 |GPIO_OSPEEDER_OSPEEDR7;
// Select AF4 (0100=0x4) to toggle I2C_SCL function on pin PB6 and I2C_SDA on pin PB7.
GPIOB->AFR[0] |= (0x4 << GPIO_AFRL_AFRL6_Pos);
GPIOB->AFR[0] |= (0x4 << GPIO_AFRL_AFRL7_Pos);
// Enable I2C peripheral clock.
RCC->APB1ENR |= RCC_APB1ENR_I2C1EN;
// Set up TIMINGR (CubeMX).
I2C1->TIMINGR = 0x00501E26;
// Peripheral Enable.
I2C1->CR1 |= I2C_CR1_PE;
}
// Variable to store the data.
uint32_t buffer[5];
// Counter.
uint32_t i = 5;
int
main()
{
initSystem();
// Set up CR2 register for data writing.
I2C1->CR2 |= (I2C_CR2_NBYTES & 1);
// 1 byte to transfer (NBYTES).
I2C1->CR2 &= ~I2C_CR2_RD_WRN;
// Write. Set 0 in RD_WRN bit for transfer direction in master mode.
I2C1->CR2 |= 0x19 << 1;
// Accelerometer address (without r/w bit).
I2C1->CR2 |= I2C_CR2_START;
// Set START bit. Master sends start condition, slave address and R/W bit.
while
((I2C1->ISR & I2C_ISR_TC) == 0);
// Wait for transfer complete.
I2C1->TXDR = 0x28;
// Put data (inernal registry address) into TXDR.
while
((I2C1->ISR & I2C_ISR_TXIS) == 0);
// Wait for TXDR is empty and ready for the new data.
// Set up CR2 register for data reading and set START bit.
I2C1->CR2 = I2C_CR2_AUTOEND | (I2C_CR2_NBYTES & 5) | I2C_CR2_RD_WRN | 0x19 << 1;
I2C1->CR2 |= I2C_CR2_START;
// Read the data.
while
(i-- > 0)
{
while
((I2C1->ISR & I2C_ISR_RXNE) == 0);
// Wait for recieve data register is ready.
buffer [i] = I2C1->RXDR;
// Copy the data from recieve data register.
}
while
(1)
{
}
}
The program execution can't pass line The line 39 should transmit an internal register address of the accelerometer. The data remain in the TXDR.
How can I check if ACK from the slave device (LSM303DLHC) is recieved?
#stm32f3-discovery #accelerometer
Labels:
- Labels:
-
Accelerometers
-
STM32F3 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-07-13 1:38 PM
Posted on July 13, 2016 at 22:38
Hi,
If you are using Standard Peripherals Library, you cancompare your generated code with one of the provided I2C Standard Lib examplesunder/content/my_st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-libraries/stsw-stm32license=1468578123html
packageand identify what you have missed. The I2C examples areavailable in this path: STM32F30x_DSP_StdPeriph_Lib_V1.2.3\Projects\STM32F30x_StdPeriph_Examples\I2C\You can refer to this
/content/ccc/resource/technical/document/user_manual/d1/02/f0/b6/1a/8a/43/de/DM00068pdf/files/DM00068pdf/jcr:content/translations/en.DM00068pdf
(Description of STM32F30xx/31xx Standard Peripheral Library) in thesection 13 Inter-integrated circuit interface (I2C), it may be helpful for you. Regards