cancel
Showing results for 
Search instead for 
Did you mean: 

I don't know how to use STEVAL-STWINMA2

D_Tomita
Associate

I possese STEVAL-STWINMA2 with STEVAL-STWINKT1B for ultrasonic measurements.

As a setup, we have attached STWINMA2 to STEVAL-STWINKT1B and installed a software "X-CUBE- MEMSMIC1".

Then, we took measurements with using UltrasoundFFT.exe in the SW_executable file of the software,

However every time I try, the only one data of the first attemption goes in to the 'Acquistitions' file,

and the other results do not show up there.

I never failed to check the box of 'save file'.

I guess that even the content of  the only data that I got does not change at all.

Even thouth I attempted to restart either my computer or STEVAL-STWINKT1B, it still does not work.

I would like you to give me any advices if you have an idea of cause of the problem.

Also, I would appreciat that I ever have an oppotunity

where you indicate me how to use  STEVAL-STWINMA2 properly.

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
SimonePradolini
ST Employee

Hello @D_Tomita 

can you share some screenshots? Can you see any kind of data in the GUI or is it frozen?

Which firmware did you flashed on the STWIN board? X-CUBE-MEMSMIC1 contains different firmware examples for STWIN board. UltrasoundFFT executable can work only with the related UltrasoundFFT firmwares. Be aware that Acoustic_SL and Microphones_Streaming examples are not compatible with the UltrasoundFFT executable.

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.