cancel
Showing results for 
Search instead for 
Did you mean: 

HT221 functional failure for above humidity sensor after long duration exposure to the air

jason239955_st
Associate III
Posted on December 15, 2017 at 17:24

Hi Sir/Mdm,@

Please advise how many heating cycle can withstand by HTS221 humidity sensor? 

Can we proposal to heat the sensor for 2nd time at 80 degree?

Regard's

Jason

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on December 16, 2017 at 11:09

What you mean by heating cycle? Usign internal heating element or heating by some external source?

The sensor operates over a temperature range from -40 °C to +120 °C, so heating to 80 °C will not hurt the sensor.