cancel
Showing results for 
Search instead for 
Did you mean: 

how to record sound from GPIO analog microphone using STM32MP157C-DK2

l_Homme
Associate II

Hello everyone,

as part of a personal project, i would like to capture analog audio signals from multiple microphones. for this I use a stm32mp157C-dk2 card.

my questions are:

  • how to record audio streams from an analog microphone connected to the gpio pins?
  • how to interface an analog microphone with a STM32MP157C card

PS: I use openstlinux

Best regards

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hello,

maybe this page would be interesting for you: https://wiki.st.com/stm32mpu/wiki/How_to_record_audio

ADC first target is not audio, and need external biasing and pre-amplifier to be used for microphones.

SPI/I2S or SAI are ok, but need external codec (See STM32MP157C-EV1 board).

Digital Microphone should be the more adapted (Using DFSDM). You could have up to 6 microphones with just using 3/4 wires, see AN5027 and STM32MP157C-EV1 board (there is 4 microphones embedded).

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here