2021-09-21 6:15 PM
2021-09-30 1:57 AM
Hi @Jsawd.1 ,
0.5g and even 1g are typical values, from datasheet Table 3 (Typical zero-g level offset accuracy).
9g is indeed a bit too high. Do you see these high values placing the board in a steady state, and soon as you start acquiring data for the first time? Or are these values the result of a system degradation?
And are you correctly reading and converting the data from LSB to milli-g? See for example
int32_t h3lis331dl_acceleration_raw_get(stmdev_ctx_t *ctx,
int16_t *val)
{
uint8_t buff[6];
int32_t ret;
ret = h3lis331dl_read_reg(ctx, H3LIS331DL_OUT_X_L, buff, 6);
val[0] = (int16_t)buff[1];
val[0] = (val[0] * 256) + (int16_t)buff[0];
val[1] = (int16_t)buff[3];
val[1] = (val[1] * 256) + (int16_t)buff[2];
val[2] = (int16_t)buff[5];
val[2] = (val[2] * 256) + (int16_t)buff[4];
return ret;
}-Eleon
2021-10-05 8:14 PM
Hi Eleon;
We are reading the values correctly, some units are fine, all units read large gs ok, its is just the noise on some of them which is an issue. It appears a little random. These are values seen in steady state, the board static.
The high values particularly occur on the z-axis.
Maybe a placement issue?, we don't know and its hard to pinpoint the casue.
many thanks
-Jon
2021-10-06 2:00 AM
Hi Jon @Jsawd.1 ,
I'm wondering whether it could be an issue related to the raw data conversion.
Did you enable the BDU bit of the CTRL_REG4 (23h) register? This prevents the output registers to be updated between MSB and LSB reading, avoiding any unwanted overlapping of the data.
-Eleon
2022-01-23 2:54 PM
Hello @Jsawd.1 - was this the problem?
we are seeing something quite odd with readings - we can run for 24 hours and suddenly, somewhere in the middle the readings will jump from 0.7 G in compeltely static state to 2.4G (after conversion). This seems to be exacerbated by the HP filter, turning it off makes this less likely but not impossible.