2023-05-09 07:35 AM
Solved! Go to Solution.
2023-05-11 11:22 PM
OK, if the problem is solved or at least answered, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-05-09 08:18 AM
Welcome, @KDoss.1, to the community!
yes, STMicroelectronics also offers gauge pressure sensors.
Just open tab Product Selector and filter according to your needs.
Hope that helps?
Regards
/Peter
2023-05-09 09:01 AM - edited 2023-11-20 05:56 AM
Thank you Peter for the prompt reply!
I am not having much luck finding the gauge pressure sensors…
Can you tell me their part numbers?
Very much appreciated!
2023-05-09 11:28 PM
I had probably misunderstood you and you want to have pressure sensors with nozzles to which you can connect a hose, for example, right?
However, STMicroelectronics only has barometric pressure sensors, as you can find them on the given URL in the tab Overview a little further down. There you can also see the waterproof sensors, whose nozzle or neck together with a rubber o-ring serves as a feed-through through a housing wall.
If the problem is solved, although perhaps not to your complete satisfaction, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-05-10 10:03 AM
No worries Peter. Thank you!
2023-05-11 11:22 PM
OK, if the problem is solved or at least answered, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter