2018-09-14 10:40 AM
Hi,
Has anyone successfully used sensortile(soldered on small cradle) with Unicleo GUI ? If yes which firmware should be used to interface sensortile with Unicleo GUI ?
In "Release Note for X-CUBE-MEMS1 Software for STM32, Expansion for STM32Cube" support for sensortile is mentioned as follows :
Projects
X-CUBE-MEMS1 Examples for SensorTile V4.3.0 (release notes)
But I could not find this particular firmware in the firmware package(X-CUBE-MEMS1 ) .
What am I missing ? Any help on above would be appreciated.
Thanks.
Solved! Go to Solution.
2018-09-19 07:06 AM
Please check X-CUBE-MEMS1-V4 package, it is legacy package of the X-CUBE-MEMS1 v5.0.0 where you can find also example for SensorTile working with Unicleo-GUI.
2018-09-19 07:06 AM
Please check X-CUBE-MEMS1-V4 package, it is legacy package of the X-CUBE-MEMS1 v5.0.0 where you can find also example for SensorTile working with Unicleo-GUI.
2018-09-24 11:28 AM
Hi,
This solution works, thanks.