cancel
Showing results for 
Search instead for 
Did you mean: 

Gone user manual, & able to port individually vibration sensor and microphone FFT data to Unicleo-GUI, Please let us know if you have a test application or reference source code to port both vibration & microphone sensor FFT data to Unicleo-GUI

SS_135
Associate II
 
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @SS_135​ , unfortunately, the goal of Unicleo-GUI is not to be open tool to display raw or processed data, but you may check the MicrophoneFFT and VibrationMonitoring example applications in X-CUBE-MEMS1, which might be used as reference code how to process data and send them to Unicleo. In particular, you can refer to:

  • MicrophoneFFT example --> Folder \STM32CubeExpansion_MEMS1_V8.1.0\Projects\STM32F401RE-Nucleo\Applications\IKS02A1\MicrophoneFFT [X-NUCLEO-IKS02A1 hardware]
  • VibrationMonitoring example --> Folder \STM32CubeExpansion_MEMS1_V8.1.0\Projects\STM32F401RE-Nucleo\Applications\IKS01A3\VibrationMonitoring [X-NUCLEO-IKS01A3 hardware]

Regards