cancel
Showing results for 
Search instead for 
Did you mean: 

Does the Sensor data logging works for Time of Flight data as well in STEVAL-BCNKT01V1 (bluecoin)?

darla14
Senior

Does the Sensor data logging works for Time of Flight data as well in STEVAL-BCNKT01V1

(bluecoin)?If no how it can be logged?Which file to look for in the workspace?I just need proximity and No Proximity data when bluecoin is mounted on the cradle.

Br,

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Eleon BORLINI
ST Employee

hi, do you refer to Sensor data logging of the Android/iOS APK (ST BLESensor app)? If so, you can try to acquire ToF data by flashing the FP-SNS-FLIGHT1 (https://www.st.com/en/embedded-software/fp-sns-flight1.html) on the Bluecoin MCU

Regards

darla14
Senior

Thanks for the quick reply.

Is there a way to log the simultaneous data for both ToF and Motion Sensors? I guess FP-SNS-FLIGHT will enable the logging option for ToF only while FP-SNS-ALLMEMS1 for Motion sensors?

Can I get both?which f/w?

Also Bluecoin doesnt have a ToF right?It is on the cradle?Neither on the coin station?

Many thanks in advance !

darla14
Senior

sorry i should have replied in the 'reply' instead of a new Answer ! :(

Eleon BORLINI
ST Employee

Don't worry =)

The FP-SNS-FLIGHT1 is able, as per the description, to perform sensor data reading, motion algorithm features demo, proximity-based hand gesture detection demo and firmware update (FOTA). You can fint the FW to be uploaded on the Bluecoin inside the folder:

en.fp-sns_flight1_firmware.zip\STM32CubeFunctionPack_FLIGHT1_V3.3.0\Projects\Multi\Applications\FLIGHT1\EWARM\STM32F446RE-BlueCoin

Regards