2018-04-24 1:31 AM
Hi..
I use STEVAL-MKI109V2(Demo board) and MKI160V1(sensor).
and i use IAR Embedded Workbench V7.20 Version..
so when i open to project file,
comming message like this..
'Broken options were detected in the project file A backup copy will be made
(see log window for detail)'
and next message is...
--> The project 'emotion' contails the unknow to 'CADI_ID'
-->
The project 'emotion' contails the unknow to 'TIFET_ID'
is it need to upgrade to over IAR 7.70 Ver??
thanks...
mailto:xfile2580@daum.net
#mki160v1 #mki109v2