cancel
Showing results for 
Search instead for 
Did you mean: 

Can u suggest me an accelerometer compatible with bridge excitation of 2V DC & the sensor is peizo resistive type with range of 50g

BRalh.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @BRalh.1​ ,

please note that ST accelerometers are capacitive and interfaces digitally (I2C/SPI/I3C/TDM) with the external world.

So, no analog (piezo) accelerometer in ST portfolio... the closest device ST has is a high-g (100g to 400g) digital accelerometer working at Vdd 2.16V (H3LIS331DL). You might check if it is suitable for your application.

-Eleon

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @BRalh.1​ ,

please note that ST accelerometers are capacitive and interfaces digitally (I2C/SPI/I3C/TDM) with the external world.

So, no analog (piezo) accelerometer in ST portfolio... the closest device ST has is a high-g (100g to 400g) digital accelerometer working at Vdd 2.16V (H3LIS331DL). You might check if it is suitable for your application.

-Eleon