cancel
Showing results for 
Search instead for 
Did you mean: 

Can a TOF sensor detect a person through a plastic case?

moon1003
Associate III

HI

We are thinking about a method for detecting people.

 

The prerequisite is that we need to detect people by penetrating a plastic case with a thickness of about 3mm (white).

The existing PIR cannot penetrate the case,

and radar sensors are expensive.

So we are considering TOF...

 

The key is to detect people by penetrating the plastic case.

I wonder if it is possible.

 

moon1003_0-1736746444564.png

 

0 REPLIES 0