Skip to main content
SWink.1
Associate
January 22, 2020
Question

Audio sampling rate mp34dt05-a

  • January 22, 2020
  • 2 replies
  • 996 views

I am using the mp34dt05-a mems microphone and receive the PDMdata stream. Now I want to do the signal processing as recommended in application note AN5027: "Interfacing PDM digital microphones using STM32 MCUs and MPUs". Thus after receiving the PDM data stream I want to do the PCM conversion as decimation stage. The decimation factor is in the range between 48 to 128 but it depends on the audio sampling frequency of the mp34dt05-a microphone. Unfortunately I can't find any note in the datasheet despite the input clock frequency which is in the range of 1,2 MHz to 3,25 MHz.

Does anybody know which audio sampling frequency is used in the mp34dt05 microphone?

    This topic has been closed for replies.

    2 replies

    Eleon BORLINI
    ST Employee
    January 22, 2020

    Hi @SWink.1​ , the MP34DT05-A device is typically tested at 2.4MHz (MIC_CLOCK), that feeds the internal delta-sigma converter. Using this MIC_CLOCK frequency with a decimation x48 you will get a PCM samples frequency of 50kSamples. Regards

    SWink.1
    SWink.1Author
    Associate
    January 22, 2020

    Thank you very much for the fast answer.