2019-07-17 5:29 AM - last edited on 2026-03-16 7:31 AM by Andrew Neil
I am using A3G4250D gyroscope in one of our project. I want to know how to convert RAW value read from register OUT_TEMP (26h) to actual temperature values?
I know that OUT_TEMP register in two’s complement format with a sensitivity of -1 LSB/°C but not able to convert to exact temperature value.
please provide the calculation to convert from RAW values to temperature value.
Thanks in Advance...!!!
2019-07-18 7:06 AM
HI @DS , please consider this caption of the AN5148 for the A3G4250D at p.43:
The A3G4250D is provided with an internal temperature sensor that is suitable for delta temperature measurement.
So it's intended to be a Delta temperature sensor... You should have a reference sensor close to the device and measure OUT_TEMP (26h) to get the right offset for the temp calculation.
However, if your application is not strictly automotive non-safety and you need accuracy in temperature, I suggest you to switch to a 6-axis module with embedded T sensor such as LSM6DSO (00h output calibrated at 25°C, on 16bit).
Regards