• Images in Profile (mƎALLEm)
  • My Images for mƎALLEm

My Images for mƎALLEm

  • Albums
  • All Images
Image Options
  • Flag Image for Review
  • Bookmark
  • Subscribe to RSS Feed

Album: Profile (mƎALLEm)

by mƎALLEm
Figure 3. Click yes to initialize the peripherals
Figure 4. Default pinout view
Figure 5. CAN activation
Figure 6. CAN pins activated
Figure 7. CAN pins on the board are free
Figure 8. CAN in Loop Back mode
Figure 9. Configuring CAN in Loop Back mode
Figure 10. Basic CAN parameters setting
Figure 11. The CAN clock is on APB1 domain
Figure 12. System clock configuration
Figure 13. Default CAN timing configuration in STM32CubeMX
Figure 14. CAN timing configuration
Figure 15. Setting the pull-up on CAN_Rx pin
Figure 16. Enable CAN RX0 NVIC interrupt channel
Figure 17. Project code generation
Figure 18. Project explorer view after generating the code
Figure 19. Compile the project
Figure 20. Configure the Saleae logic analyzer digital channel 0 input in CAN mode
Figure 21. CAN configuration with Saleae logic analyzer
Figure 22. Start a debug session of the application in STM32CubeIDE
Figure 23. Adding TxData and RxData to the Live Expressions in STM32CubeIDE
Figure 24. Running the application on STM32CubeIDE
Figure 25. Zoom-out of the CAN frames captured by the logic analyzer
Figure 26. Zoom-in on the first CAN frame sent by the STM32 and captured by the logic analyzer
Figure 27. Tx and Rx buffers are changing in live in the STM32CubeIDE debugger
SofLit_0-1729078448084.png
Figure 1. Pierce oscillator structure
Figure 2 HSE_gm_products.png
Figure 3 LSE_gm_products.png
Figure 4. A screenshot from CX3225GA8000D0PTVCC crystal datasheet
Figure 5. A screenshot from STM32H743 datasheet showing Gmcritmax value
Figure 6. A screenshot from LFXTAL081620 crystal datasheet
Figure 7 Cp_H7.png
Figure 8.png
Figure 7.png
CAN.png
Figure 7. Standard capacitor value in this case is 10 pF
Figure 2. HSE transductance by product
Figure 3. LSE transductance by product
mALLEm_0-1743945799983.png
Disco test.jpg
Figure 1. The CAN bit time
Figure 2. CAN bit time generation on STM32
Figure 3. CAN prescaler field in CAN_BTR register
Figure 4. RCC clock configuration example
Figure 5. Time quantum shown by STM32CubeMX
Figure 6. The CAN instances are located on APB1 domain
Figure 7. Time segment 1 and Time segment 2 fields in CAN_BTR register
Figure 8. STM32F439ZI MCU selection in STM32CubeMX
Figure 9. Setting HSE in Bypass mode in STM32CubeMX
Figure 4 CX3225GA8000D0PTVCC_spec.png
Previous
Figure 4. A screenshot from CX3225GA8000D0PTVCC crystal datasheet
Next
Added ‎2025-03-07 4:08 AM
0 Kudos
Figure 4. A screenshot from CX3225GA8000D0PTVCC crystal datasheet
Posted in: How to select a compatible crystal and load capacitors for STM32 with layout guidelines - ( ‎2025-04-17 6:00 AM )