2018-11-19 02:15 AM
I would like to know if it is possible to create a device compatible with Zigbee Smart Energy 1.2a standard from the STM32WB55xx devices.
I have seen the library STRF4CE for Zigbee implementation but I am not sure if it works for this version of standard or if it is possible to use this library with the chip.
In the case this solution is feasible, I would like to know if there is any reference project that I could use as a starting point for this application.
Thanks and best regards,
2018-11-22 06:43 AM
ACK?