2022-04-04 2:28 AM
I have a few X-Nucleo-IDB05A1 boards, and when I test them on the X-Cube64 board, some work and some don't. So I checked it, and like the attached picture file, the Trace Code and Bulk ID are different.
Trace code XN915011 is fine,
11540270 doesn't work at all.
What's the matter?
2022-04-07 5:50 AM
HI @BSalt.1 ,
Do you confirm Jumper and solder bridges configuration are exactly similar on both boards ?
Thanks,
Sebastien.
2022-04-10 9:46 PM
@Sebastien DENOUAL
Hi,
Yes the idb05A1 board has only one 2pin jumper block and some 0 ohm jumpers that need to be replaced by soldering, both types of boards are factory-set.
Thanks,
Ewing.