cancel
Showing results for 
Search instead for 
Did you mean: 

wifi_reset Problem with IDW01M1

arturdav87
Associate II
Posted on December 14, 2016 at 07:57

I'm using the STM32F411RE board with the IDW01M1 WiFi expansion module. I run some examples from en.x-cube-wifi1_firmware.zip lib.

However, all example code I run always fail during the wifi_init()--> wifi_reset() call where it just hangs in this while loop:

while(IO_status_flag.WiFi_WIND_State.WiFiHWStarted != WIFI_TRUE)

{

__NOP(); //nothing to do

}

but WiFiHWStarted never gets set to WIFI_TRUE.

Maybe i dismissed some wiring conncetions (the expantion connected via wires to eval board)?

I have JP3 set in the 1-2 position (which it is). I also have JP4 set in the 1-2 position.

I have connceted 3.3v to CN7 pins 12&

Thanks,

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This discussion is locked. Please start a new topic to ask your question.
33 REPLIES 33
Posted on October 27, 2017 at 09:11

In my case it looks like it was a hardware problem. I put an new X-NUCLEO-IDW01M1 and the hanging issues stopped!

Posted on November 05, 2017 at 08:52

Same here... Changing the 

X-NUCLEO-IDW01M1

 solved the problem.. 

I need to now check what is the issue with the old board. 

I did tap the uart lines and check in the oscilloscope  but I could not see any data transmitted. 

Thanks 

Raghuram 

Posted on November 05, 2017 at 08:53

Changing the 

X-NUCLEO-IDW01M1

 solved the problem..

Thanks 

Raghuram 

Posted on November 24, 2017 at 06:46

Hi Yoann,

I did a little more digging by reading the WIND messages coming over UART from the SPWF01SA. 

I see that the board in which the issue is present, I donot see

+WIND:32:WiFi Hardware Started 

message.

But in the new 

X-NUCLEO-IDW01M1, I receive this message and after this everything works fine.

Any idea what could be causing the SPWF01SA to not send this message? Could it be an issue in the Hardware? 

Has anyone faced this problem?

The old board version is 3.4 (SPWF01S-150410-c2e37a3).

Thanks for the help

Regards,

Raghuram