cancel
Showing results for 
Search instead for 
Did you mean: 

Teseo-VIC3D

rasmus_cplace
Associate

Hi

I have some question regarding the Teseo-VIC3D information which I cannot find.

1. The Teseo-VIC3D should have its own asm330 unit which internally is interfaced over SPI, right? 

2. Is it possible to interface the ASM330 as if it where an external hw unit?

3. Or just to get the values?

3a. If yes how often?

3b. and is it calibrated, raw or both values?

4. I can see there are several commands to set uart/nmea port speed
- CDB-ID 102 – NMEA port baud rate setting
- $PSTMCFGPORT on UART

are there any difference in which to use?

 

/Rasmus

0 REPLIES 0