cancel
Showing results for 
Search instead for 
Did you mean: 

STUSB1602 - BMC interface required to advertise power sourcing ability? BMC clock frequency?

JBegr.1
Associate

I am evaluating the STUSB1602 in combination with a STMF103 in a dual-role port, UFB (usb-device) application. In source mode, the device should provide type-c current 5V 3A or 5V 1,5A. Do I have to connect the BMC interface to advertise power sourcing ability?

Unfortunately, the datasheet is not clear to me about the BMC interface. In addition to my main question, if I do need the BMC interface at all for my application, I can not find any information about the SPI CLOCK frequency the STUSB outputs?

Best regards,

Jakob

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0