cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to use custom bootloader to update firmware of BlueNRG-2 chip over SPI or I2C peripheral?

KSoni.1
Associate

I have a custom board with multiple MCUs and a BlueNRG-2 chip. I have a binary file of BlueNRG-2 in an external flash connected over SPI or I2C. 

I need to replace the existing application binary with the one stored in the external flash.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Winfred LU
ST Employee

It is possible.

You may want to reference BLE_OTA_ServiceManager project for customizing your own bootloader to use SPI or I2C flash accordingly.