2017-11-01 6:20 AM
I can connect to network using
wifi_connect function without any issues.
priv_mode = WPA_Personal;
status = wifi_connect('NETWORK','password', priv_mode);When i try to configure module with firstset, it associates with AP but then it disconnects, here are the WIND messages:
+WIND:57:Received SSID is NETWORK
+WIND:57:Received Auth mode is 2+WIND:57:Received PWD is password+WIND:57:Received IBSS Auth type is 0+WIND:57:Received Dhcp setting is 1+WIND:57:Received Mode is 1+WIND:2:Reset+WIND:1:Poweron (160129-c5bf5ce-SPWF01S)+WIND:13:ST SPWF01S IWM: Copyright (c) 2012-2015 STMicroelectronics, Inc. All rights Reserved.+WIND:3:Watchdog Running+WIND:0:Console active+WIND:32:WiFi Hardware Started+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:19:WiFi Join:C0:A0:BB:AB:46:A2+WIND:25:WiFi Association with 'NETWORK' successful+WIND:41:WiFi Disassociation:14+WIND:40:WiFi Deauthentication:6
+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)then it goes in scanning loop and never connects again.
My AP is configured to use WPA/WPA2.
#wifi-spwf01sa2017-11-04 3:25 AM
Is the module able to connect by AT-commands (no firstset)?
ps: please update to FW3.5.3
2017-11-22 3:02 AM
Hi all,
I am facing similar problem.i have updated the firmware to 3.5.3.Still the WiFi module is not able assign IP address.and restarting again
2017-11-22 8:45 AM
Did you call AT+S.WIFI=0 before AT&W? Try to enable the radio again (AT+S.WIFI=1) before AT&W.
Please dump AT&V and AT+S.STS here (module seems in IDLE mode).