2016-04-05 9:13 AM
I need to send complete (and receive) custom packet through the module SP1ML to cummunicate with another SPIRIT1 board (protocol is fixed). This protocol is based on ''Basic Packet'' (no StAck nor Wmbus) with :
12 bytes preamble 2 bytes Sync Word variable length payload No address sent No Control sent CRC 0x8005 Is it possible to obtain this with the SP1ML module? We used the STEVAL board to communicate without problems. Is it possible to do this with SP1ML with original Fw ? Thank you very much Best Regards Simone #spirit1-sp1ml-dongle #spirit1-sp1ml