2022-03-29 06:24 AM
Solved! Go to Solution.
2022-03-29 06:54 AM
Welcome, @AKuma.42, to the community!
perhaps you have overlooked the data, which is of course included in the data sheet of the USBL6-4SC6, page 2, table 1 and 2:
The USBLC6-4SC6 was developed for USB 1.1 and USB 2.0, so it can protect the 5V lines commonly used there.
Does it answer your questions?
Regards
/Peter
2022-03-29 06:54 AM
Welcome, @AKuma.42, to the community!
perhaps you have overlooked the data, which is of course included in the data sheet of the USBL6-4SC6, page 2, table 1 and 2:
The USBLC6-4SC6 was developed for USB 1.1 and USB 2.0, so it can protect the 5V lines commonly used there.
Does it answer your questions?
Regards
/Peter
2022-03-29 07:31 AM
Hi Peter,
Thanks for your response.
Need one clarification whether Operating junction temperature and Operating temperature is same or it's different. If it's same this is the answer for my question. If not then need to know the same.
Thanks,
Arun
2022-03-29 07:36 AM
The ambient temperature is important for components where power dissipation occurs and self-heating takes place. With these protection diodes, this (usually) only happens in the case of protection and only lasts for an extremely short time, so that no significant heating occurs.
In this respect, the junction temperature can be equated with the ambient temperature.
Regards
/Peter
2022-03-29 09:17 PM
Thanks for the clarification Peter....
Thanks,
Arun
2022-03-29 11:47 PM
Great!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2022-03-30 04:14 AM
Select as best doesn't mean to edit the topic and add "Solved:" in front of it, but clicking Select as best under the most favourite answer.