Skip to main content
Associate
February 10, 2025
Solved

Simpler uC with CAN feature

  • February 10, 2025
  • 2 replies
  • 562 views

Hello community!

What are the simplest ST uC with CAN feature?

Yours suggestions will be welcome!

Many thanks and Regards!

 

This topic has been closed for replies.
Best answer by mƎALLEm

Hello @zpedro and welcome to the community,

That depends on what do you mean by "the simplest ST uC".

First, there are two CAN flavors: bxCAN peripheral (CAN2.0) and FDCAN peripheral (CANFD).

Second, STM32F0, STM32F1, STM32F2, STM32F3, STM32F4, STM32F7 families have bxCAN peripheral

while STM32G4, STM32H7, STM32H5 etc .. have FDCAN peripheral.

So if you mean by simple not a very complex MCU I can suggest STM32F0 family based on Cortex-M0:

You can use STM32CUbeMx or STM32Finder tools to select the suitable MCU for your application:

SofLit_0-1739188147485.png

Hope that helps.

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
February 10, 2025

Hello @zpedro and welcome to the community,

That depends on what do you mean by "the simplest ST uC".

First, there are two CAN flavors: bxCAN peripheral (CAN2.0) and FDCAN peripheral (CANFD).

Second, STM32F0, STM32F1, STM32F2, STM32F3, STM32F4, STM32F7 families have bxCAN peripheral

while STM32G4, STM32H7, STM32H5 etc .. have FDCAN peripheral.

So if you mean by simple not a very complex MCU I can suggest STM32F0 family based on Cortex-M0:

You can use STM32CUbeMx or STM32Finder tools to select the suitable MCU for your application:

SofLit_0-1739188147485.png

Hope that helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
zpedroAuthor
Associate
February 14, 2025

Hi SofLit, many thanks for the tip! ;)

Regards,

José