Skip to main content
JKo
Associate III
December 5, 2022
Question

S2-LP:How to reliably abort RX while in transition through LOCK state

  • December 5, 2022
  • 0 replies
  • 572 views

In my channel hopping application the radio is configured to start RX following any frequency change. However the frequency change may be followed by a TX instead so I may need to abort the RX soon after issuing CMD_RX from READY. Table 50 gives the response time for READY -> LOCK_RX -> RX as 111 us.

AFAIK, depending on whether the radio is in LOCK_RX or RX, CMD_READY or CMD_SABORT is required to transition the radio back to READY in preparation for CMD_TX. There is a potential race condition here between querying the current state which could return LOCK and issuing CMD_READY instead of CMD_SABORT. This leads to the radio not accepting the CMD_READY from the RX state and CMD_TX later also failing.

Is there a reliable way to abort the RX without looping to get the current state?

What states can be reported in MC_STATE0 during the state transition from READY to RX?

    This topic has been closed for replies.