cancel
Showing results for 
Search instead for 
Did you mean: 

S2-LP - Excelent results obtained with TCXO and BALF-SPI2-01D3

enrico239955
Associate II

Hi folks,

we just completed a custom RF interface board for our product.

It's a simple SPI-to-Antenna board with TCXO and BALF, in the 862-868 MHz band.

The TCXO is powered by an LDO at 1.8 Volt. This allows us to use a battery.

The S2-LP is powered externally at 3.3 Volt (internally it uses its DC/DC at 1.8 Volt)

The RF performances are great:

The CW signal has a variance of just 300 Hz aournd the carrier at 868 MHz

TX: we got 4 dBm better than the same board with a quartz crystal

RX: we got 2 dBm better than the same board with a quartz crystal

TCXO

1.8 V 50 MHz+/- 0.5 ppm -40, +85 Celsius)

Manufacturer: KDS

PN: DSB211SDN

It can be purchased in Italy from CODICO.

BALUN:

MANUFACURER: ST

PN: BALF-SPI2-01D3

PCB:

MANUFACTURER: MD srl Italy

LAMINATE: FR4 common

LAYERS: 4

L1 = RF signals

L2 = GND

L3 = Just 3 traces of VDD (*)

L4 = SPI signals

(*) No power plane at all. The layer is empty except for 3 traces of VDD

To achieve this result we followed all the ST guidelines.

In particular, the BALUN needs to be routed according to ST guidelines.

No VDD traces must be routed below the S2-LP chip or the BALF.

Enrico Migliore

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0