2019-01-11 5:50 AM
The S2-LP DK package comes with pre-compiled binarys that are used with the GUI application(S2LP_CLI_NUCLEO_L0.hex/ bin). Is the source code available for this CLI? I want to port this to my custom board (containing a STM32G microcontroller), so I can use the GUI to evaluate the performance.
2021-05-14 12:32 AM
Kindly following
2021-05-16 7:34 PM
Yes, please download S2-LP DK:
Currently L0 and L1 are supported.
Efforts to port it to STM32G is needed.