2016-12-08 12:13 AM
Hi,
I was wondering that if it is possible to delete the HTML and CGI file system from the module.?
P.S: I can see from the documentation that it is possible to disable/enable the feature. My concern is to permanently delete the files.
#cgi2016-12-10 6:17 AM
Hi,
cannot delete files inside STM32 flash (so, HTML and/or CGI). The ones marked as 'I' from AT+S.FSL command.
You can delete HTML inside external flash, if using SPWF01Sx.11, by AT+S.HTTPDFSERASE. The ones marked as 'E' from AT+S.FSL command.
Regards
jerry
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.