2016-12-05 12:32 PM
Hello folks,
while experimenting with an idw01m1 module, I am experiencing deauthentication with the message:
WIND:40:WiFi Deauthentication 3
With the '2015' firmware, the module was unable to reconnect until WiFi was turned off and on.
With latest (2016) firmware the situation has improved a bit, and the module automatically reconnects.
I strongly suspect this behaviour has something to do with a timeout because:
1) it happens only if there is no data exchange
2) it happens exactly and systematically after 300 seconds from the last RX/TX.
Yet, I wasn't able to find a parameter either in the module or in the router to change it.
To connect, I execute this sequence after a factory reset:
at+s.scfg=wifi_wpa_psk_text,<password>
at+s.ssidtxt=<my SSID>
at+s.scfg=wifi_priv_mode,2
at+s.scfg=ip_use_dhcp,1
at+s.scfg=wifi_mode,1
at+s,wifi=0
at+s.wifi=1
Commands are written via console, so I am sure to wait for the correct answer.
With the automatic reconnection, the situation is not that bad. I just fear that DHCP can assign a different IP when the module re-authenticates. This would cause undesired behaviour in my application.
I am using a WPA2 personal authentication. The router is an ASUS N55U.
Hints?
2016-12-10 6:02 AM
Ciao Giuseppe,
sorry for delay.
Release 2015 had some limitation on scan activity (this is why module was not able to join without a reset).
About latest FW:
- there is no timeout on module like this: 300 seconds
- reason 3 is never used from module (1, 2, 4, 5, 6, 7 and 8 are used)
Here (
https://supportforums.cisco.com/document/141136/80211-association-status-80211-deauth-reason-codes
) I found reason 3 meaning. I suspect AP is deauthenticating the module. If you can, log a wireshark session. You should find a deauth packet from AP to module.Suggestion: I found this behavior on 'big' network's AP (i.e., public networks). After some time, AP deauth module if no traffic is found. To avoid this behavior'
- try to change AP settings
- or, AT+S.PING someone before timeout (i.e., every 256 seconds).
Suggestion #2: change configuration variables after AT+S.WIFI=0, and before AT+S.WIFI=1.
Regards
jerry
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.