2017-01-06 3:37 AM
Hello ST,
it seems that the escape_seq parameter does not work as expected in the IDW01M1.
There are some discrepancies between the user manual and the obtained results. Please have a look at my transcript:
12:16:15.761 [TX] - at+s.scfg=escape_seq,at+miao<CR>
12:16:26.101 [RX] - OK
+WIND:61:Incoming Socket Client:192.168.0.218
+WIND:60:Now in Data Mode
12:25:49.307 [TX] - at+miao
12:25:49.807 [RX] - +WIND:59:Back to Command Mode
12:26:05.899 [TX] - at+miao
12:26:10.363 [TX] - at+miao<CR>
12:26:10.595 [RX] - ERROR: Command not found
12:26:13.700 [TX] - AT+S.<CR>
12:26:13.703 [RX] - +WIND:60:Now in Data Mode
So, it seems that:
1) escape_seq only changes the data->command sequence, but not the command->data
2) when in command mode, you need to send a to activate the sequence, despite the fact that the manual states the opposite.
Some more information:
♯ nv_model = SPWF01SA1
♯ nv_serial = 3915D31697
♯ version = 160129-c5bf5ce-SPWF01S
Giuseppe
#x-nucleo-idw01m1 #spwf01sa1 #escape-sequenceSolved! Go to Solution.
2017-01-07 7:19 PM
Ciao Giuseppe,
escape sequence is used to exit data mode. Once in command mode, you need to run 'at+s.' command to come back into data mode again. It's a command, not An escape.
j
2017-01-07 7:19 PM
Ciao Giuseppe,
escape sequence is used to exit data mode. Once in command mode, you need to run 'at+s.' command to come back into data mode again. It's a command, not An escape.
j
2017-01-12 1:50 PM
Ciao Gerardo,
after reading your comment, I checked carefully the manual. In facts it confirms what you say.
Perhaps I can suggest to give some more emphasis to the 'note' that describes escape sequence. Anyway, the description is correct.
Thanks
G.
2017-01-13 3:19 AM
Please use 'Mark Correct' button to close the issue
2017-01-13 9:14 AM
I'd like to... but how? I don't see any button or action that allows me to do so :(
I can mark a message as useful, like it, give a badge, but can't find a way to 'close' the question.
2017-01-13 9:34 AM
Understand. Probably because you opened a 'Discussion', that is not a 'Question'. I see a different icon, without question mark.
No problem
j