cancel
Showing results for 
Search instead for 
Did you mean: 

ICCID and Activation of ST4SIM-300M eSIM

saharhaghdadi
Associate II

Hi,

I’m currently working with an ST4SIM-300M eSIM and testing it for an IoT application.

I was able to read the following ICCID from the device:
89019990001234567893

I wanted to ask if anyone knows which operator or profile this ICCID belongs to. Also, I’m not sure how the activation process should work for the ST4SIM-300M.

Does it come with any initial bootstrap profile for network access, or do I need to provision a profile first before it can connect?

AT%PINGCMD=0,"8.8.8.8"
OK
AT+CPIN
ERROR
AT+CSQ
+CSQ: 99,99

OK
AT%PDNSET?
%PDNSET: 1,,IPV4V6,,,,,0,0,0

OK
at+cops?
+COPS: 0

OK
at+cops=0

At the moment I’m not able to get network connectivity, so any guidance on the correct activation/provisioning steps would be really helpful.

Thanks in advance!

0 REPLIES 0