2019-04-24 2:16 AM
I am using BLENRG-MS for the same.
2019-04-24 7:24 PM
Hi,
With BLE Mesh, the messages are managed flooded to the network.
You don't even have to implement by yourselves.
Options are available to either
or
Best Regards,
Winfred
2019-06-01 4:38 AM
Hi,
I want to send Digital Microphone data from one device to other two devices. So which BLE and micro-controller should I use for better performance? I am totally new to this and I need some help on coding too. So please let me know how can I start for the same.
Thanks and regards,
Om Patel
2019-06-01 7:14 AM
@Winfred LU
We have just received STM32WB55 Nucleo pack and I found that there is only one IDE workspace is available in (en.stm32cubewb\STM32Cube_FW_WB_V1.0.0\Projects\NUCLEO-B55.Nucleo\Applications\BLE\BLE_MeshLightingDemo)
and that is EWARM and when I tried to import it into atollic TrueStudio then I am getting following error
"Description Resource Path Location Type Fatal error[LMS001]: License check failed. Use the IAR License Manager to BLE_MeshLightingDemo Unknown C/C++ Problem"
Do we required EWARM licence to import EWARM Workspace into others like Atollic Truestudio or STM32CubeIDE? or can you please provide BLE_MeshLightingDemo in Atollic Truestudio or STM32CubeIDE?
Regards,
VK Verma