2022-03-10 12:15 AM
2022-03-10 2:56 AM
Hmmmm, the connection is from bluenrg1 to bluenrg1 and it is my own board. I can verify that there is a connection by blinking LEDs when the two are connected. By pending action? Do you mean the peripheral side?
2022-03-10 2:59 AM
This is the code to program the peripheral ble, there is nothing pending (i think). Unless I am missing any callback functions needed to grant access? I didn't set any security though... if that is a possibility. And since I am not reading anything yet, I didn't think that aci_gatt_allow_read() is necessary. Althought, I do have it in my peripheral code already.
2022-03-10 4:36 AM
Hi,
By chance, does simialr code return same erro ron STEAL board (STEVAL-IDB07V1) ?
Did you performed a HW bringup of your PCB ? see AN4818
If you run server code on your BlueNRG-1 board : are you able to connect using smartphone debug APP surch as BLE_Scanner ?
Regards,
Sebastien
2022-03-10 6:32 AM
Hmmmm i dont have a STEVAL-IDB07V1 at hand.
But I am able to connect to the server/peripheral using an app such as the BLE Scanner app
2022-03-10 7:10 AM
Would there be any known patches for the discovery and read functions by any chance? Because I am using the BlueNRG-1 2 DK 3.2.1... I tried using the latest version but since I'm using old code. I ran into some conflicts.
If not, hci_le_connection_complete_event() should provide the connection handle and it should work with aci_gatt_disc_all_primary_services() without giving an error through aci_gatt_proc_complete_event () right?
If its a yes to the above, would there be a way to test aci_gatt_read_char_value() on the server locally? Just to test that I am using the function correctly. Or not?