2021-10-27 2:31 AM
Hey Team, iv had some issues trying to modify the BLE_HID_Peripheral example.
Iv modified the report descriptor and can confirm it works on another BLE ic.
The only things iv changed outside the report descriptor are just the config_hid function.
At hidSetDeviceDiscoverable it returns BLE_STATUS_INVALID_ADV_FLAGS
" * @brief The discoverability flags in the advertising data are not coherent
* with the discoverability mode set in the advertising configuration"
but to my understanding here the hiddevice_init sets that up
//################################################
//TEST
//###############################################
uint8_t Configure_HidPeripheral(void)
{
uint8_t ret;
batteryService_Type battery;
devInfService_Type devInf;
hidService_Type hid;
connParam_Type connParam;
/* HID Peripheral Init */
connParam.interval_min = 9;
connParam.interval_max = 10;
connParam.slave_latency = 0;
connParam.timeout_multiplier = 300;
/**
* @brief Initializes the HID Device with Peripheral Role and
* sets the public address.
* @param IO_Capability Sets the device IO capabilities. Possible value are:
* - IO_CAP_DISPLAY_ONLY
* - IO_CAP_DISPLAY_YES_NO
* - KEYBOARD_ONLY
* - IO_CAP_NO_INPUT_NO_OUTPUT
* - IO_CAP_KEYBOARD_DISPLAY
* @param connParam Connection parameter to send to the
* HID Host after bonding/service discovery
* @param dev_name_len Device name length
* @param dev_name Device name
* @param identity_address_type The type of own adress. It must be one between
* @ref PUBLIC_ADDR or @ref STATIC_RANDOM_ADDR.
* @retval Status of the call.
*/
ret = hidDevice_Init(IO_CAP_DISPLAY_ONLY, connParam, sizeof(dev_name), dev_name, STATIC_RANDOM_ADDR);
if (ret != BLE_STATUS_SUCCESS) {
PRINTF("Error in hidDevice_Init() 0x%02x\n", ret);
return ret;
}
/* Set the HID Peripheral Security */
/**
* @brief Configures the device for LE Security Mode 1 and either Security Level 2 or 3
* To set the Security Level 2 the MITM mode param shall be equal to FALSE, all the other params are ignored.
* To set the Security Level 3 the MITM mode param shall be equal to TRUE, the other params shall be used to
* signal if the device uses a fixed PIN or not.
* @param MITM_Mode MITM mode. TRUE to set the security level 3, FALSE to set the security level 2
* @param fixedPinUsed TRUE to use a fixed PIN, FALSE otherwise. If the MITM_Mode param is FALSE, this param is ignored
* @param fixedPinValue PIN value
* @retval Status of the call.
*/
ret = hidSetDeviceSecurty(TRUE, TRUE, 123456);
if (ret != BLE_STATUS_SUCCESS) {
PRINTF("Error in hidSetDeviceSecurty() 0x%02x\n", ret);
return ret;
}
/* Set the HID Idle Timeout */
hidSetIdleTimeout(IDLE_CONNECTION_TIMEOUT);
/* Set the TX Power */
ret = aci_hal_set_tx_power_level(0, 24);
if (ret != BLE_STATUS_SUCCESS) {
PRINTF("Error with aci_hal_set_tx_power_level() 0x%02x\n", ret);
return ret;
}
/**** Setup the GATT Database ****/
/* Battery Service */
battery.inReportMap = FALSE;
/* Device Information Service */
memcpy(devInf.manufacName, "ST Micro", 8);
memcpy(devInf.modelNumber, "0001", 4);
memcpy(devInf.fwRevision, "0630", 4);
memcpy(devInf.swRevision, "0001", 4);
devInf.pnpID[0] = 0x01;
devInf.pnpID[1] = 0x30;
devInf.pnpID[2] = 0x00;
devInf.pnpID[3] = 0xfc;
devInf.pnpID[4] = 0x00;
devInf.pnpID[5] = 0xec;
devInf.pnpID[6] = 0x00;
/* HID Service */
//hid = hid_param;
hid.bootSupport = FALSE; // no boot support
hid.reportSupport = FALSE; // i would guess it would support a report characteristic
hid.num_reports = NUM_REPORTS; // What defines the amount of reports characteristics ? (is it referring to byte allocation for the report ?)
hid.reportReferenceDesc = reportReferenceDesc;
hid.reportReferenceDesc[0].ID = REPORT_ID;
hid.reportReferenceDesc[0].type = INPUT_REPORT;
hid.reportReferenceDesc[1].ID = REPORT_ID;
hid.reportReferenceDesc[1].type = OUTPUT_REPORT;
hid.isBootDevKeyboard = FALSE;
hid.isBootDevMouse = FALSE;
hid.externalReportEnabled = FALSE; // not sure was 0
hid.includedServiceEnabled = FALSE;
hid.informationCharac[0] = 0x01;
hid.informationCharac[1] = 0x01;
hid.informationCharac[2] = 0;
hid.informationCharac[3] = 0x01;
hid.reportDescLen = sizeof(reportDesc); /** Report Descriptor length */
hid.reportDesc = reportDesc; /** Report Descriptor */
//#########################
//adds all services
// Adds the Primary service and the characteristics associated
// * for the battery, device information and hid services.
//#########################
ret = hidAddServices(&battery, &devInf, &hid);
if (ret != BLE_STATUS_SUCCESS) {
PRINTF("Error in hidAddServices() 0x%02x\n for &battery ", ret);
return ret;
}
//#########################
//discoverable
//#########################
/* Set the HID Peripheral device discoverable */
/**
* @brief Starts the peripheral device discoverable mode. This mode is ended
* when either the upper layer issues a command to terminate the procedure
* using the command hidTerminateDiscoverableMode() or the
* timeout happens (timeout value is 180 s).
* @param mode Discoverable mode to use:
* - LIMITED_DISCOVERABLE_MODE
* - GENERAL_DISCOVERABLE_MODE
* @param nameLen Local name length. Max 20
* @param name Local name value
* @retval Status of the
*/
ret = hidSetDeviceDiscoverable(LIMITED_DISCOVERABLE_MODE, sizeof(dev_name), dev_name);
if (ret != BLE_STATUS_SUCCESS) {
PRINTF("Error in hidSetDeviceDiscoverable() 0x%02x\n", ret);
return ret;
}
PRINTF("HID gamepad Configured\n");
BSP_LED_Off(BSP_LED1);
/* Button Init */
BSP_PB_Init(USER_BUTTON, BUTTON_MODE_EXTI);
return BLE_STATUS_SUCCESS;
}
Main:
int main(void)
{
uint8_t ret;
/* System initialization function */
if (SystemInit(SYSCLK_64M, BLE_SYSCLK_32M) != SUCCESS)
{
/* Error during system clock configuration take appropriate action */
while(1);
}
/* Configure IOs for pwer save modes */
BSP_IO_Init();
/* Configure I/O communication channel */
BSP_COM_Init(BSP_COM_RxDataUserCb);
/* BlueNRG-LP stack init */
/* Application demo Led Init
BSP_LED1 = Sensor configuration led
BSP_LED3 = Connection led
*/
BSP_LED_Init(BSP_LED1);
BSP_LED_Init(BSP_LED2); // Led on when not sleeping
BSP_LED_Init(BSP_LED3);
BSP_LED_On(BSP_LED1);
BSP_LED_On(BSP_LED2);
BSP_LED_Off(BSP_LED3);
/* Clock Init */
Clock_Init();
ModulesInit();
/* Set HID Service params */
//setDefaultHidParams();
/* Configure HID Peripheral and put the device in discoverable mode */
ret = Configure_HidPeripheral();
if (ret != BLE_STATUS_SUCCESS) {
PRINTF("Error in configure_hid_peripheral() 0x%02x\n", ret);
}
while(1) {
ModulesTick();
/* Application Tick */
APP_Tick();
/* Device Power Save Management Procedures */
//DevicePowerSaveProcedure();
}
}