2021-12-20 1:33 AM
Solved! Go to Solution.
2021-12-21 11:59 PM
You can look at the X-NUCLEO-GNSS1A1 as an example, where, in addition to the inductor L2 (56nH) and the block capacitor C9 (56pF), a bidirectional single line ESD TVS protection diode is used. You can find all information under the tab CAD Resources: schematics, bom, etc.
Regards
/Peter
2021-12-20 4:32 AM
Please have a look at UM2832, section 8.2. where the coupling of an active antenna is shown. It is a different TESEO module, but the principle is identical. The DC supply of the antenna is fed in via an LC element, decoupled from the received signal. In addition, the UM2832 shows how Ant_OFF can optionally be used to switch this DC.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-12-20 10:14 PM
Thanks, Peter!
Please suggest us how to select the values for the DC coupling components (inductor & bypass capacitor & AC coupling component(capacitor in the RF line).
Regards,
Faize
2021-12-21 11:59 PM
You can look at the X-NUCLEO-GNSS1A1 as an example, where, in addition to the inductor L2 (56nH) and the block capacitor C9 (56pF), a bidirectional single line ESD TVS protection diode is used. You can find all information under the tab CAD Resources: schematics, bom, etc.
Regards
/Peter