2016-03-30 01:48 AM
Good morning,
I have some problems regarding firmware update. When I try to update firmware via serial link, I obtain this message:''Error sending message 0x31 to device'' as show also in the image: Someone can help me?Stefano2016-03-30 02:25 AM
Ciao Stefano,
seems FLASH is corrupted...Can you please try an update through standard (GUI-based) FlashLoaderDemonstrator tool? Let me knowjerry2016-03-30 03:34 AM
Thank you for reply, Gerardo.
With ''flash demonstrator'' the issue is resolved. I can reprogram one module (I have two of this, one return unknown device) , performing the entire flash download. At the end the progress bar show in green. After that I release the BOOT0 pin and repower the module, but this doesn't write on the serial. Why?2016-03-30 04:24 AM
Because you erased the bootloader too.
Starting address of application is 0x08002800.Please contact your local distributor to recover that module.2016-03-30 06:10 AM
It isn't possible to have bootloader binaries to flash on the board?
Stefano2016-03-30 06:26 AM
Please ignore last post, my distributor sended me the boot binaries.
Thanks a lot for your help.Stefano