Associate II
October 13, 2015
Question
Data loss using SPWF01SA (multiples of 2kiB)
- October 13, 2015
- 18 replies
- 3419 views
Posted on October 13, 2015 at 10:31
Hi,
i'm using the SPWF01SA with high baud rates (460k or 920k) and continuous transmission at maximum speed. From time to time (minutes for 460k, all the time for 920k), data sent via UART is not transmitted via WIFI. It is always a multiple of 2kiB that is lost. RTS/CTS is working fine (see attached picture; upper channel is RX, lower channel RTS (both at WIFI-module)). Firmware should be up-to-date; at least I can use ADC command.Thanks for your help,Georg