cancel
Showing results for 
Search instead for 
Did you mean: 

Can't terminate connection attempt after incoming connection established on BlueNRG-MS

nick239955_stm1_st
Associate II

I have discovered an issue when trying to use aci_gap_terminate_gap_procedure( GAP_DIRECT_CONNECTION_ESTABLISHMENT_PROC ) after previously calling aci_gap_create_connection(...) to connect to a slave device. The issue only occurs if an incoming connection is established between calling the create and terminate functions. In this case aci_gap_terminate_gap_procedure returns 0x0C (ERR_COMMAND_DISALLOWED) instead of 0x00 (BLE_STATUS_SUCCESS) which it does usually.

I am currently using v7.2c of the stack. I have just found out that v7.3 is now available but the release note does not indicate that this issue has been fixed?

0 REPLIES 0