cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-ms doesnt follow Bluetooth core specification?

bjornpaulstrom
Associate III
Posted on February 21, 2017 at 21:57

Hello, I am using a BlueNRG-ms (IDB05A1) flashed to latest fw 7.2c trying to develop a HID compliant mouse for Windows.

However when pairing with windows using only the basic GATT and GAP(no other services or changes) from the BlueNRG GUI there are some problems, Windows says:

Device (0x280E1003C2A) is not Compliant with the Bluetooth Core Specification: previous attribute was a (Characteristic), current attribute is a (Descriptor).

Is this a bug or is Windows wrong? BlueNRG-ms page states:

'

The BlueNRG-MS is a very low power Bluetooth low energy (BLE) single-mode network processor, compliant with Bluetooth specification v4.1.'

Is this a cause for concern?

#stm32 #bluenrg-ms #windows #idb05a1 #hid #bluetooth #ble
1 REPLY 1
bjornpaulstrom
Associate III
Posted on February 22, 2017 at 15:41

bump