2023-02-20 09:46 AM
described in table 8 of BlueNRG-M2 datasheet. But there is no description of what the Mode is.
Is it a pin or SW configuration or model type?
Solved! Go to Solution.
2023-02-22 05:38 PM
mode 000 = GPIO mode
mode 001 = Serial0 mode
mode 010 = Serial1 mode
mode 101 = Serial2 mode
Those are the operating modes that I/O pins can be configured.
The modes are set in registers GPIO-MODE0 ~ GPIO-MODE3,
at offsets GPIO_BASE_ADDR+0x2C ~ GPIO_BASE_ADDR+0x38
See also BlueNRG-2 datasheet, chapter 3.12 GPIO
2023-02-22 05:38 PM
mode 000 = GPIO mode
mode 001 = Serial0 mode
mode 010 = Serial1 mode
mode 101 = Serial2 mode
Those are the operating modes that I/O pins can be configured.
The modes are set in registers GPIO-MODE0 ~ GPIO-MODE3,
at offsets GPIO_BASE_ADDR+0x2C ~ GPIO_BASE_ADDR+0x38
See also BlueNRG-2 datasheet, chapter 3.12 GPIO
2023-02-23 02:35 AM
I read there is a pin, but could not find it. This explains it. If I set sections differently it is at least palatially configurable then.Thanks for fast replay.