cancel
Showing results for 
Search instead for 
Did you mean: 

BLUE NRG-TILE : how to setup debugging through truestudio with examples

AMeta
Associate II

Hey,

Im using the STEVAL-BCN002V1 Along with a nucleo board connected to it.

i've imported the example projects into trustudio as i couldnt get them working in stm32ide.

The problem im having is im unsure on the process to setup the debugging (after building) , the setup sheet doesnt really go into detail on the process just on how to connect up the two device.

im planning on buying the addon for this board as well, but is there a clean process to get the live debugging going on truestudio ?

Thankyou,

Andreas

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0